EIP.PLLSTATE

Description

This parameter reads the state of the Phase-Locked Loop (PLL). The EIP.PLLSTATE can be queried in WorkBench terminal to report the current value and state of the PLL. Value 6 (Locked) indicates the AKD2G-SPI PLL is synchronized with the PLC.

Value

Description

0

Idle (not locked)

1

Acquiring lock

2

Searching for reference period

3

Searching for phase lock

4

Searching for frequency lock

5

Fine adjust

6

Locked

7

Fault

Versions

Action Version Notes
Implemented 02-10-00-000

General Information

Type

Read Only

Units

N/A

Range

0 to 7

Default Value

0

Data Type

Integer

See Also EIP.PLLMODE

Stored in Non-Volatile Memory

No

Variants Supported

EtherNet/IP drives: AKD2G-SPI

Industrial Ethernet

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

3901

1

3901 (0xf3d)

EIP.PLLSTATE

Unsigned8

Read Only

Yes